Outputs of Motor Controller Plug & Drive Motor | NANOTEC

The motor controllers and Plug & Drive motors have open collector outputs. To switch a load or PLC, you require a relay according to this circuit diagram. The flyback diode is required. Please don't exceed the maximum switching current or the maximum voltage of the selected controller. You can find this information in the respective manual.  

SMCI35:  A load/PLC cannot be connected with this controller.

Back

Questions? Comments?

Do you have questions or remarks about this article?

Contact support