Example Program Rockwell Add-Ons

This example helps you set up our controllers with a Rockwell SPS via the EtherNet/IP interface, assuming that a CompactLogix PLC and Studio 5000 Software version 20 or newer from Rockwell are being used. 
Rockwell and EtherNet/IP are widely used in the packaging industry, among others.

Example Program

This program can be used to test positioning and speed modes
4 MB
Back

Questions? Comments?

Do you have questions or remarks about this article?

Contact support