About us

Ein Blick in unser Büro

About us

Nanotec GmbH&Co. KG has been providing its customers with dependable support in the implementation of drive solutions since 1991. Our motors and positioning controls are available in a wide range of products and offer the appropriate solution for practically all work tasks.

Well thought-out construction, compliance with tight production tolerances and strict quality control during all stages of the process allow us to provide top-quality and durable drive solutions.

As well as compliance with the requirements of the standards and relevant sets of regulations, certification in accordance with the latest standard ISO 9001:2000 by the TÜV Management Service documents the consistent customer orientation of our processes and the successful efforts towards continuous improvement of internal and external procedures.

Our Vision: Fast and easy - but with a personal touch

The requirements of drive solutions are diverse and a standard motor or power electronics „out-of-the-box” can only rarely be used if optimum results are to be achieved. Therefore, we offer customer-specific versions of our motors and positioning controls in relatively small numbers. Motors and positioning controls in relatively small numbers. Our engineers develop the optimum mechanical and electronic design of a customized solution on request.

In-house production and broad-based warehousing mean we can react flexibly and quickly to customer wishes.

On time and reliable

Our performance shows that we do not regard reliability and timeliness as empty words, but as an obligation. For example, by adherence to schedules: Nanotec meets 98 % of all confirmed delivery dates. We endeavor to keep any delays as short as possible in the remaining 2 %. In many cases, we are even able to meet preferred delivery dates.

An achievement that our customers appreciate: The more than 4000 motors and 200 positioning controls we deliver each week speak for themselves, as do the reputations of our well-known customers:

Einige unserer namhaften Kunden

Contact information

Nanotec Electronic GmbH & Co. KG

Gewerbestraße 11
D-85652 Landsham
Telephone ++49 89 900 686-0
Fax ++49 89 900 686-50

ISO 9001 ISO-Zertifikat Nanotec 2010