Driver
Download >> Driver
RS485-USB converter
This driver is required when the NANOTEC ZK-RS485-USB converter is used.
Further information about the converters can be found on the converter line product page .
Driver for Windows 7, XP, Vista (5,2 MB)
Driver for Windows 2000 (3,2 MB)
RS232-USB converter
This controller is required when the NANOTEC ZK-RS232-USB converter is used - NOT FOR THE SMCI35 CONTROLLER!
Further information about the converters can be found on the converter line product page . This converter is only required if you have the ZK-RS485-RS232 converter and want to establish a connection to the USB interface.
Driver for WIN XP, 2000 (1.9 MB)
Driver for Windows VISTA (1.8 MB)
USB - RS232-3,3V - Converter
For connecting the Steppermotor controller SMCI35 with a PC over USB you need to download and install this driver.
USB drive for SMCI controls
The SMCI33-1 and SMCI32-1 positioning controls with USB connection require a special controller in order to establish the communication of the module via the serial interface.
You can download this controller here:
Drivers for SMCP33-EVA
If you want to operate the SMCP33 evaluation board with the USB connection, you will need this driver.